Channels view parameters (RTD devices)
The
Channels
view for RTD devices includes these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Input Type | Indicates the RTD input type. |
Input Range | Indicates the input range as follows:
|
High Signal | Displays the high signal values. |
Low Signal | Displays the low signal values. |
Units (Signal) | Shows the unit of measurement for High Signal and Low Signal . |
High Engineering | Specifies the appropriate scaling high units. Set the value between -32768 and 32767. The default value is 500 (1734-IR2, 1738-IR2IM12) and 300 (1734-IR2E). High Engineering is disabled in Run mode and when Temperature Unit is set to one of these values:
|
Low Engineering | Specifies the appropriate scaling low units. Set the value between -32768 and 32767. The default value is 0. Low Engineering is disabled in Run mode and when Temperature Unit is set to one of these values:
|
Units (Engineering) | Shows the unit of measurement for High Engineering and Low Engineering and for the channel’s input value. |
Digital Filter | Specifies the desired filter time constant, in milliseconds (ms). Set the value between 0 (default) and 10,000. Digital Filter is only disabled in Run mode. |
Disable Alarms | Determines whether process alarms are generated.
|
Provide Feedback