CJ Calibration view parameters
The
CJ Calibration
view includes these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel to which this configuration applies. |
Calibration Range | Displays the calibration range as 1000 ohms to 3000 ohms . |
Calibration Status | Shows the status of the calibration per channel as the calibration occurs. Valid values include:
|
Start Calibration | Starts the calibration process while online. |
Provide Feedback