Calibration view parameters (input devices)
The
Calibration
view for input devices includes these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Calibration Range (Voltage and Current) | Displays the calibration range:
Calibrate Range is enabled in Run mode and is only available while online. |
Calibration Range (RTD and Thermocouple) | Displays the calibration points. For RTD devices, the calibration point is:
For thermocouple devices, the calibration point is:
Calibrate Range is enabled in Run mode and it is only available while online. |
Calibration Status | Shows the status of the calibration per channel as the calibration occurs. Valid values include:
|
Start Calibration | Select to start the calibration process. Start Calibration is available in Run mode.Tip : Start Calibration is available when online. |
Provide Feedback