Alarms view parameters
The
Alarms
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
|---|---|
Disable All Alarms | Select to disable all process alarms. Tip : Selecting Disable All Alarms also disables other features for Alarm, such as Latch Process Alarms and all the Process Alarm features. Unlatch All and Unlatch remain enabled. |
Latch Process Alarms | Select to latch all process alarms. |
High High Limit | Choose the desired high high process alarm value. The range is -32768–32767. The default value for Current is 16793. The default value for Voltage is 9800. The default value for RTD and Thermocouple is 32767. |
High Limit | Choose the desired high process alarm value. The range is -32768–32767. The default value for Current is 16547. The default value for Voltage is 9500. The default value for RTD and Thermocouple is 32767. |
Low Limit | Choose the desired low process alarm value. The range is -32768–32767. The default value for Current is 3113. The default value for Voltage is 500. The default value for RTD and Thermocouple is -32768. |
Low Low Limit | Choose the desired low low process alarm value. The range is -32768–32767. The default value for Current is 2867. The default value for Voltage is 200. The default value for RTD and Thermocouple is -32768. |
Unlatch All | Select to unlatch all the process alarms. Unlatch All is only available while online. |
Unlatch | Select to unlatch only the corresponding alarm named to the left of Unlatch .Unlatch is only available while online. |
Provide Feedback