Time Synchronization view
- On the explorer bar, select
Devices. - InDevices, double-click the controller to open the device profile.
- In the device profile, selectTime Synchronization.
Use the
Time Synchronization
view to view time synchronization status and enable or
disable time synchronization on the controller. Enabling time synchronization allows the
controller to participate as a clock in the system time. It also allows the controller to
become a master clock for the system, or become a master clock in the chassis.If the controller is the grandmaster clock, all devices connected to the controller
synchronize with the clock of the controller. The
Time Synchronization
view displays
details for the device that is acting as the grandmaster clock.Provide Feedback