Points view parameters
The
Points
view includes these parameters:Input Points
Parameter | Description |
|---|---|
Mode | Select the device operation when input state changes to High:
|
Filter time off | Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid. |
Filter time on | Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid. |
Output Points
Parameter | Description |
|---|---|
Mode | Select the device operation when output state changes to High:
|
Output state in program mode | Determines the behavior of each output when the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored and the output behaves according to these:
|
Output state in fault mode | Determines what happens to the output of each point after a communication fault occurs and the device enters Communications Fault mode.
|
When communication fails in program mode | Determines the output action if communication fails in program mode:
|
Provide Feedback