Antenna view parameters

The
Antenna
view includes these parameters:
Parameters
Parameter
Description
Value
Frequency Band
Select the frequency band for the antenna.
58UHF-TR-100-SR15US
  • 902.75 through 914.75MHz
  • 915.25 through 927.25MHz
58UHF-TR-200-LR50US
  • 902.75 through 914.75MHz
  • 915.25 through 927.25MHz
58UHF-TR-100-SR15EU
  • 865.7MHz
  • 866.3MHz
  • 866.9MHz
  • 867.5MHz
58UHF-TR-200-LR50EU
  • 865.7MHz
  • 866.3MHz
  • 866.9MHz
  • 867.5MHz
Command sequence error action
Select to continue or stop when an error is detected for commands with multiple sequence.
Tip
: Command sequence error action is hidden when Continuous Inventory mode is selected on Device Definition.
  • Continue sequence
  • Stop sequence
Radio Frequency (RF) Power
  • Read power
    The RF Power for Inventory or Read commands.
  • Write power
    The RF Power for Write, Lock, or Kill commands.
Select RF Power:
  • US15 and EU15: 10.0 through 24.0
  • US50 and EU50: 10.0 through 30.0
Device must be inhibited to calibrate device
Select Calibrate to launch the Radio Frequency Power Calibration Wizard.
Calibrate
Antenna
Antenna polarity
  • Circular (default)
  • Vertical linear
  • Horizontal linear
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal