Module Properties dialog box - Safety Module Info tab parameters
The Safety Mo
dule Info
tab includes these parameters:Parameter | Description |
Identification | Displays the following identification information about the module.
The name displayed in the Product Name field is read from the module. This name displays the series of the module. If the module is a 1756-L1 module, this field displays the catalog number of the memory expansion board (this selection applies to any controller catalog number even if additional memory cards are added.) |
Major/Minor Fault Status | For a digital module, these options are available:
For an analog module, these options are available:
For other modules, these options are available:
|
Internal State Status | Displays the current operational state.
If you selected the wrong module from the module selection tab, this field displays a hexadecimal value. A textual description of this state is only given when the module identity you provide is a match with the actual module. |
Configured | Displays a yes or no value indicating whether the module has been configured by an owner controller connected to it. Once a module has been configured, it stays configured until the module is reset or power is cycled, even if the owner drops connection to the module. This information applies to I/O modules only and does not apply to adapters, scanners, bridges, or other communications modules. This value does not apply to safety applications. |
Owned | Displays a yes or no value indicating whether an owner controller is currently connected to the module. This information applies to I/O modules only and does not apply to adapters, scanners, bridges, or other communications modules. This value does not apply to safety applications. |
Module Identity | These options are available:
This field does not take into account the Electronic Keying or Minor Revision selections for the module that were specified on the General tab. Generic modules, such as the 1756-MODULE, always show a Mismatch because the configured Generic Key does not match any target device. |
Diagnostics | Accesses the Diagnostics dialog box which contains diagnostic information. |
Refresh | Retrieves and displays the latest values from the module. |
Reset Module | Initiates a reset operation on the module, which returns the module to its power-up state by emulating the cycling of power. Important : Resetting a module closes all connections to or through the module, which may result in loss of control.Tip : Some modules may return an error if a reset is attempted. |
Provide Feedback