Overriding output state inhibits safety state of the point
WARNING:
Selection of "Hold" for
Output State During Program Mode and Communications Fault
Mode
prevents the output point from going to the safe state, making the output point
not suitable for a SIL or PL rated safety function.Set
Output State During Program Mode and Communications Fault Mode
to "Off" to
allow points to go to safe state
IMPORTANT:
TÜV Rheinland has approved GuardLogix 5580 and Compact GuardLogix 5380 controller systems
for use in safety-related applications where the deenergized state is always considered to
be the safe state. You must ensure configuration of each channel of the safety IO module
is set for "Off" under the
Output State During Program Mode and Communications Fault
Mode
selection to consider those output points as part of any equipment’s safety
function.Changing the setting of the
Output State during Program Mode and Communications Fault Mode
inhibits the safety state transition of the point when the settings change from Off
to Hold
Select
Apply
or OK
to proceed with the change, select No
to cancel the
change, or select Help
to view the Help.Provide Feedback