Module Properties dialog box - Test Output Points parameters

The
Test Output Points
for the input module includes these parameters.
Tip:
The parameters that appear depend on which module is being configured. Parameters that do not apply to the module are hidden.
Parameter
Description
Point
The point number to which this configuration applies. The number of points depends on which module is being configured.
Point Mode
Determines the mode of the test output for the point. Available selections depend on the module.
  • Not Used
    - Test output is not used.
  • Pulse Test
    - Use the test output point as a pulse test source.
  • Power Supply
    - Use the test output as a power supply.
  • Muting Lamp
    - The test output connects to an indicator lamp. Only available when
    Muting Lamp Points
    on
    General
    page is set to
    Point 02, Point 03
    , or
    Point 02 and 03
    .
Diagnostics
Opens the
Point Diagnostics
dialog box to view diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal