Test source is invalid
An invalid test source has been selected. Only test outputs configured as
Safety Pulse Test
can be used as test sources. A test output can be associated with 0, 1, or 2 safety input channels. Check the configuration and make the required modifications.Provide Feedback