Channel X Diagnostics dialog box parameters (Generic ASCII Receive/Transmit)
When the device is online, the
Channel
dialog box shows real-time statistics for the Generic ASCII Receive/Transmit communication. This information is used for performance and error management.X
DiagnosticsParameter | Description |
|---|---|
Sent Character Count | Number characters sent to the serial port. |
Received Character Count | Number of characters received from the serial port. |
Reset Diagnostics | Resets diagnostics for channel. Supported on Major Revision 2 and higher. |
Provide Feedback