Overview view
The 5069-SERIAL device provides communication connections to serial devices. It has two channels that are independent of each other. In the
Device definition
dialog box, use the Overview
view to configure device definition properties and to specify the protocol for each channel.
TIP:
If the channel is not used, set
Channel
to X
Disabled
. If Channel
is set to X
Modbus Master
or Modbus Slave
, use the Channel
views in X
Device definition
to set up the Modbus Master and Modbus Slave.Provide Feedback