Create a Modbus Slave data mapping table
In
Device definition
, use the Channel
view to create and configure the data mapping table for the Modbus Slave.X
- Modbus SlavePrerequisites
- The device must be offline.
To create a Modbus Slave data mapping table
- On the tab for the device, selectOverview, and then selectDevice definition.
- InDevice definition, selectOverview, and then selectModbus Slaveas the protocol to use on the channel.
- From the navigation ofDevice definition, selectChannelthat hasXModbus Slaveas the selected protocol.
- In theChannelview, configure the parameters, and then selectX- Modbus SlaveOK.
Provide Feedback