Channel X - Modbus Master view parameter
In
Device definition
, when Channel
is set to X
Modbus Master
, the Channel
view includes these parameters:X
- Modbus MasterParameter | Description |
|---|---|
![]() | Moves the selected commands up in the list. IMPORTANT : If you move the command up, adjust the program to reflect the new command location. Otherwise, a return error occurs upon validation. |
![]() | Moves the selected commands down in the list. IMPORTANT : If you move the command down, adjust the program to reflect the new command location. Otherwise, a return error occurs upon validation. |
Command | Indicates the command being configured. |
Communication Method | Specifies the communication method for the command. Available options are:
Tip: Parameters are unavailable when the communication method is disabled. |
Data Type | Specifies the data type for the command. Available options are:
|
Function Code | Specifies the function of the command. Available options depend on Data Type :
|
Slave Address | Specifies the node address of the Modbus Slave device. Valid value is 0–247. Tip: For broadcast command, set Slave Address to 0. |
Modbus Address Offset | Specifies the offset to the actual Modbus Address. Valid value is from 0 through 65535. |
Data Length | Specifies the number of data points being read. The valid data length values depend on the Data Type and the Function Code . |
Poll Interval | Specifies the number of seconds between each time the command is executed when in Continuous mode.For example, if the Poll Interval is set at 10, the Modbus Master waits 10 seconds before executing the command again.Valid value is from 0 through 32767. Tip: This parameter is unavailable when the Communication Method is Conditional . |
Swap Mode | Specifies the arranging of the received/send data from the Modbus Slave. Possible available options:
|
Fault Enable | Determines whether or not to overwrite the received data with a Fault Value if the read command fails.Select the checkbox to overwrite the received data with the Fault Value .Tip: This parameter is unavailable when the Function Code is a write command. |
Fault Value | Specifies the value to replace the received data. |
Remaining connection data | Displays the remaining connection data as the command list is configured. When Connection 1 is not able to fit the next command, Connection 2 is used, and remaining Connection 1 data is set to 0. When Connection 2 is not able to fit all the commands, remaining Connection 2 data shows how many bytes (in negative number) cannot fit. |
Provide Feedback