Channel X - Modbus Master view parameters

The
Channel
X
- Modbus Master
view defines the characteristics of the Modbus Master.
The
Channel
X
- Modbus Master
view includes these parameters:
Parameter
Description
Modbus Format
Determines whether the Modbus transmission format is
Modbus RTU
or
Modbus ASCII
.
The default is Modbus RTU.
Response Timer
Defines the minimum amount of time a Modbus client waits for a response from the server before a new transmission can begin.
Valid value is from 0 through 3600000 ms. The default is 200 ms.
Broadcast Pause
Specifies the delay after the data broadcast.
Valid value is from 0 through 3600000 ms. The default is 200 ms.
Inter-Frame Timeout
Specifies maximum delay time to receive data for the Remote Terminal Unit (RTU).
Tip: This parameter is available only when
Modbus Format
is set to
Modbus RTU
.
Retry Count
Specifies the maximum number of times to retry the request.
Valid value is from 0 through 127. The default is 0.
Diagnostics
When online, opens the diagnostics dialog box to view diagnostic counters for performance and error management with the Modbus Master.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal