Channel X - Generic ASCII Transmit view parameters

Use the
Channel
X
- Generic ASCII Transmit
view to configure the
Generic ASCII Transmit
mode.
The
Channel
X
- Generic ASCII Transmit
view includes these parameters:
Parameter
Description
Swap Mode
Determines how the data transmitted to the serial port is arranged. The swapping is done before the device sends output data. Available options are:
  • No Change
    (default)
  • Word Swap
    (ABCD = CDAB)
  • Byte Swap
    (ABCD = BADC)
  • Word and Byte Swap
    (ABCD = DCBA)
Termination Mode
Determines the usage of the termination delimiters in the data. Available options are:
  • Ignore End Delimiter
    (default). End delimiter is ignored and treated as ordinary data.
  • Exclude
    . End delimiter is not included in the send data.
  • Include
    . End delimiter is searched and is always the last byte of the data.
Tip: The termination delimiter is only applied when Ox.ASCII.TxDataLength = 0.
Termination Delimiter 1
Specifies the channel's first termination delimiter. The termination delimiter is used to signal the end of the data. Valid values are:
  • 7 bit - $00 to $7F
  • 8 bit - $00 to $FF
Termination Delimiter 2
Specifies the channel's second termination delimiter. Valid values are:
  • 7 bit - $00 to $7F, $FF
  • 8 bit - $00 to $FF
Tip: To use only the first termination delimiter to signal the end of the data, set
Termination Delimiter 2
to
$FF
.
Diagnostics
When online, opens the diagnostics dialog box to view diagnostic counters for performance and error management with the Generic ASCII Receive/Transmit communication.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal