Configure test output parameters

Configure test output parameters for the input device.
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, under the
    Test Output Points
    section, configure the following parameters as needed:
    • Point Mode
      . Select the output mode of the test output.
    • Diagnostics
      . If online, select diagnostic-icon to view diagnostic information.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal