Ptxx Diagnostics view parameters (5034-IB8S)
The
Ptxx Diagnostics
view includes these parameters:
Parameter | Description |
|---|---|
Fault Exists | Displays whether a fault is present. |
Data Uncertain | Displays whether the module is operating outside the designed
operating range. |
Field Power | Displays whether field power is present on the point. |
Field Power On Timestamp | Displays the timestamp of the last time field power turned on
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Field Power Off Timestamp | Displays the timestamp of the last time field power turned
off in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Point Off to On Timestamp | Displays the timestamp of the last time the point turned on
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Point On to Off Timestamp | Displays the timestamp of the last time the point turned off
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Short Circuit Fault | Displays whether a short circuit (short to high) fault is
present on the point. |
Short Circuit Fault Timestamp | Displays the timestamp of the last short circuit fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Internal Fault | Displays whether an internal fault is present on the
point. |
Internal Fault Timestamp | Displays the timestamp of the last internal fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Over Temperature Fault | Displays whether an over temperature fault is present on the
point. |
Over Temperature Fault Timestamp | Displays the timestamp of the last over temperature fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Critical Temperature Fault | Displays whether a critical temperature fault is present on
the point. |
Critical Temperature Fault Timestamp | Displays the timestamp of the last critical temperature fault
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Provide Feedback