Points view parameters (5034-OB8S)
The
Points
view includes these parameters:
Parameter | Description |
|---|---|
Point | Displays the point number to which this configuration
applies. |
Point Operation Type | Determines whether the points function individually or as
connection pairs.
|
Point Mode | Defines the mode of the point.
|
Enable No Load Diagnostics | Enable or Disable No Load Diagnostics for the output
point. When enabled, No Load Diagnostic is performed if output is
Off. |
Diagnostics | Open the Diagnostics dialog, which contains diagnostic
information. |
Latch Fault until Reset via Output Tag | Enable or disable latching fault until reset via output
tag.
|
Provide Feedback