Overview view parameters

The
Overview
view includes these parameters:
Parameter
Description
Series
Displays the series of the device.
Revision
Displays the revision of the device.
Electronic Keying
Displays the electronic keying that is used for the device.
Connection
Displays the connection type and the communication format.
Channel Assignments
Displays the operation mode that is assigned for each channel.
Device Definition
Opens Device definition dialog to change the revision, electronic keying, channel mode, and other device-specific values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal