Channels view parameters
The
Channels
view includes these parameters:Parameter | Description |
|---|---|
Port | Displays the module port numbers. |
Channel | Displays the module channel numbers. |
Mode | Displays the operation mode for the channel. |
Digital Output State During Program Mode | Determines the behavior of each output when the controller transitions to Program
Mode or Inhibit mode. While in Program Mode or Inhibit mode, outputs from the
controller are ignored and the output behaves as follows:
|
Digital Output State During Communication Fault Mode | Determines what happens to the output of each point after a communication fault
occurs and the module enters Communications Fault Mode.
|
Digital Input Filter Time Off → On | Defines how long an Off to On input transition must remain in the On state before
the device considers the transition valid. |
Digital Input Filter Time On → Off | Defines how long an On to Off input transition must remain in the Off state
before the device considers the transition valid. |
Counter Preset | Displays the value, set in the output tag Preset, to use for counter preset. The
value can range from 0…2,147,483,647. |
Counter Rollover at Preset | Determines the action that is taken when the input tag Count reaches the output
tag Preset value.
|
Diagnostics | Opens the Diagnostics dialog to view diagnostic information. |
Provide Feedback