IO-Link Event Log parameters
The
IO-Link Event Log
includes these parameters:Parameter | Description |
|---|---|
Timestamp | Displays the timestamp of the event that occurred in YYYY-MM-DD-HH:mm:ss:mmm
format.
|
Type | Displays the type of event that is received from the IO-Link device. |
Mode | Displays the mode of the event that is received from the IO-Link device. |
Description | Displays the description of the event based on the Event Code. |
Event Code | Displays the code for the event that is received from the IO-Link device. |
Clear Log | Clears the Event Log for this port. |
Refresh | Updates the Event Log for this port. |
Provide Feedback