Chxx – Digital Output view parameters
The
Chxx – Digital Output
view includes these parameters:Parameter | Description |
|---|---|
Output State in Program Mode | Determines the behavior of each output when the controller transitions to Program
Mode or Inhibit mode. While in Program Mode or Inhibit mode, outputs from the
controller are ignored and the output behaves as follows:
|
Output State in Communication Fault Mode | Determines what happens to the output of each point after a communication fault
occurs and the module enters Communications Fault Mode.
|
When Communication Fails in Program Mode | Determines the output action if communication fails in Program Mode.
|
Enable No Load Diagnostics | Determines whether No Load detection is enabled. No Load detects whether a signal
wire has been disconnected from one of its terminals or the RTB has been
removed. |
Diagnostics | Opens the Diagnostics dialog to view diagnostic information. |
Provide Feedback