Chxx – Digital Input view parameters

The
Chxx – Digital Input
view includes these parameters:
Parameter
Description
Input Filters
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input Filters
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Diagnostics
Opens the Diagnostics dialog to view diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal