Chxx – Digital Input, Timestamp, Fallback view parameters
The
Chxx – Digital Input, Timestamp, Fallback
view includes these parameters.Parameter | Description |
|---|---|
Disable Channel | Select this checkbox to disable the channel temporarily. When the channel is disabled, both IO-Link communication and Digital Input on the
channel are deactivated. This parameter can be changed while online. |
Input Filters Off → On Filter Time | Defines how long an Off to On input transition must remain in the On state before
the device considers the transition valid. |
Input Filters On → Off Filter Time | Defines how long an On to Off input transition must remain in the Off state
before the device considers the transition valid. |
Enable Timestamp Latching | Determines whether timestamps are latched.
|
Capture Timestamp for Off → On Input Transition | Determines whether a timestamp is recorded for the Off to On input
transition. |
Capture Timestamp for On → Off Input Transition | Determines whether a timestamp is recorded for the On to Off input
transition. |
Enable Chatter Detection | Sets chatter detection. When enabled, chatter from a device that is connected to
one of its inputs (for example, rapid transitions from a failed contact) is
ignored. Chatter can cause the device to timestamp invalid input transitions. Typically,
chattering signals cause inputs to transition falsely many times in a relatively
short period of time. |
Chatter Count | Determines the number of acceptable input transitions that can occur in a given
time period before considering the input to be chatter. Valid values are 2…127. |
Chatter Time | Determines the amount of time, from 1…10,000 milliseconds, within which the
number of input transitions are counted. |
Diagnostics | Opens the Diagnostics dialog to view diagnostic information. |
IO-Link Event Log | Opens the IO-Link Event Log dialog to view the IO-Link port events. |
Disable and Delete Data Storage | Select to disable Data Storage and delete the master copy of the Data Storage on
this port. This temporarily disables Data Storage for maintenance purpose. Whether Data
Storage is disabled when the IO-Link device connection is running is defined in
the Device Definition view of the IO-Link Device AOP.
TIP:
Disabling Data Storage is only allowed when
the connection to the IO-link device is Inhibited.
|
Provide Feedback