Chxx Diagnostics view parameters (Digital Input, Digital Output, IO-Link Modes)
The
Chxx Diagnostics
view includes these parameters. You cannot see all
parameters, as some are specific to the channel mode you selected.
Parameter | Description |
|---|---|
IO-Link Status | Displays the status of the connected device. |
Fault Exist | Displays whether a fault is present on the channel. |
Data Uncertain | Reserved |
Field Power | Displays whether the field power is present. |
CQ Short Circuit Fault | Displays whether the channel has a CQ short circuit fault. |
SSV Short Circuit Fault | Displays whether the channel has an SSV short circuit fault. |
No Load Fault | Displays whether the channel has a No Load fault. |
Short Circuit Fault | Displays whether the channel has a short circuit or overcurrent
fault. |
Field Power On Timestamp | Displays the timestamp of the last time field power turned on in
YYYY-MM-DD-HH:mm:SS.mmm format.
|
Field Power Off Timestamp | Displays the timestamp of the last time field power turned off in
YYYY-MM-DD-HH:mm:SS.mmm format.
|
CQ Short Circuit Fault Timestamp | Displays the timestamp of the last CQ Short Circuit fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
|
SSV Short Circuit Fault Timestamp | Displays the timestamp of the last SSV Short Circuit fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
|
No Load Fault Timestamp | Displays the timestamp of the last No Load fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
|
Short Circuit Fault Timestamp | Displays the timestamp of the last Short Circuit fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
|
Provide Feedback