Chxx - Counter view parameters
The
Chxx - Counter
view includes these parameters:Parameter | Description |
|---|---|
Input Filters Off → On Filter Time | Defines how long an Off to On input transition must remain in the On state before
the device considers the transition valid. |
Input Filters On → Off Filter Time | Defines how long an On to Off input transition must remain in the Off state
before the device considers the transition valid. |
Counter Preset | Displays the value, set in the output tag Preset, to use for counter preset. The
value can range from 0…2,147,483,647. |
Counter Rollover at Preset | Determines the action that is taken when the input tag Count reaches the output
tag Preset value.
|
Diagnostics | Opens the Diagnostics dialog to view diagnostic information. |
Provide Feedback