Scaling and the scaling equation
Input scaling allows the translation of electrical signal units into engineering units. The
module returns the High Engineering value when the High Signal value is present at the
input. Similarly, the module returns the Low Engineering value when the Low Signal is
present and all other values in a linear fashion, depending on the signal present at the
input.
For voltage input types, scaling is defaulted to a 1:1 relationship between the signal
values and the engineering units, allowing the module to return the actual value of the
signal present on the input.
For current input types, scaling is defaulted to return 0...100% for a corresponding 4...20
mA or 0...20 mA signal on the input.
For RTD and Thermocouple input types, scaling values display units based on sensor type or
temperature units (°F, °C, K, or °R) when the selected sensor type is not Ohms or mV.
High Signal values must be greater than Low Signal values.
Scaling Equation
Provide Feedback