Calibration view parameters

The
Calibration
view include these parameters:
Parameter
Description
Channel
Displays the channel number to which this configuration applies.
Calibration Range
Displays the value currently configured for the channel. Values display according to the Input Type selected.
Calibration Gain
Displays the calibration gain reported by the device.
Calibration Offset
Displays the offset in signal units as reported by the device.
Last Calibration Date
Displays the last calibration date for the channel.
Calibration Status
Displays the status of the calibration per channel as the calibration occurs. Valid values include:
  • OK
  • Error
Start Calibration
Select to begin the calibration process.
Start Calibration is enabled when the module is inhibited or online with the controller in Program Mode.
Revert to Factory Calibration
Calibration values gets reverted to the factory default values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal