Revert to Factory Calibration view parameters

Parameter
Description
Channel
Displays the channel number to which you can revert the current calibration values.
Revert to Factory Calibration
Defines which channel calibration values to be reverted to factory calibrated vaules.
Calibration Range
Displays the value currently configured for the channel. Values display according to the Input Type selected.
Current Calibration Gain
Displays the current calibration gain values reported by the module.
Current Calibration Offset
Displays the current offset in signal units reported by the device.
Calibration Status
Displays the status of the calibration for each channel.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal