PtXX - Output, Scheduled view parameters
Parameter | Description |
|---|---|
Program state | Determines the behavior of each output when the controller transitions to Program mode.
|
Parameter | Description |
|---|---|
Leave outputs in Program Mode state | Leaves output in Program mode state when communications fail in Program mode. |
Change outputs to Fault Mode state | Changes output to Communication Fault mode state when communications fail in Program mode. |
Parameter | Description |
|---|---|
Communication fault state | Determines what happens to the output of each point after a
communication fault occurs and the device enters Communications Fault mode.
|
Communication fault state duration | Determines the length of time the output state is held before
transitioning to the Final Fault State.
|
Final communication fault state | Determines whether the device transitions to On or Off after the Fault
Mode Output State Duration elapses. The default final state is Off. If you choose
Forever for Duration, the Final State setting is ignored and the device retains its
current Fault mode state.
|
Parameter | Description |
|---|---|
Diagnostics | Opens the diagnostics dialog box to view diagnostics information. |
Provide Feedback