PtXX - Input view parameters

Input Filters
Parameter
Description
Member Name
Value
Off → On filter time
Specifies a value by which to delay the transition from Off to On. This delay is useful for filtering out transients in noisy environments.
C.Ptxx.InputOffOnFilter
  • 0 µs (default)
  • 5 µs
  • 10 µs
  • 20 µs
  • 50 µs
  • 100 µs
  • 200 µs
  • 500 µs
  • 1 ms
  • 2 ms
  • 5 ms
  • 10 ms
  • 20 ms
  • 50 ms
On → Off filter time
Specifies a value by which to delay the transition from On to Off. This delay is useful for filtering out transients in noisy environments.
C.Ptxx.InputOnOffFilter
  • 0 µs (default)
  • 5 µs
  • 10 µs
  • 20 µs
  • 50 µs
  • 100 µs
  • 200 µs
  • 500 µs
  • 1 ms
  • 2 ms
  • 5 ms
  • 10 ms
  • 20 ms
  • 50 ms
Other
Parameter
Description
Diagnostics
Opens the diagnostics dialog box to view diagnostics information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal