PtXX - Input, Output - Input view parameters
Parameter | Description | Member Name | Value |
|---|---|---|---|
Off → On filter time | Specifies a value by which to delay the transition from Off to On.
This delay is useful for filtering out transients in noisy environments. | C.Ptxx.DI.InputOffOnFilter |
|
On → Off filter time | Specifies a value by which to delay the transition from On to Off.
This delay is useful for filtering out transients in noisy environments. | C.Ptxx.DI.InputOnOffFilter |
|
Provide Feedback