PtXX - Input, FIFO view parameters
Parameter | Description | Member Name | Value |
|---|---|---|---|
Off → On filter time | Specifies a value by which to delay the transition from Off to On.
This delay is useful for filtering out transients in noisy environments. | C.Ptxx.InputOffOnFilter |
|
On → Off filter time | Specifies a value by which to delay the transition from On to Off.
This delay is useful for filtering out transients in noisy environments. | C.Ptxx.InputOnOffFilter |
|
Parameter | Description | Member Name | Value |
|---|---|---|---|
Capture timestamp for Off → On input transition | Determines whether to capture a timestamp when the input transitions
from Off to On. | C.Ptxx.CaptureOffOnEn | 0 = Do not capture (default) 1 = Capture |
Capture timestamp for On → Off input transition | Determines whether to capture a timestamp when the input transitions
from On to Off. | C.Ptxx.CaptureOnOffEn | 0 = Do not capture (default) 1 = Capture |
Parameter | Description | Member Name | Value |
|---|---|---|---|
Enable chatter detection | Sets chatter detection. When enabled, chatter from a device connected
to one of its inputs (for example, rapid transitions from a failed contact) is
ignored. Chatter can cause the device to timestamp invalid input transitions.
Typically, chattering signals cause inputs to transition falsely many times in a
relatively short period of time. | C.Ptxx.ChatterCount | 0 = Disabled (default) 2...127 = Enabled |
Chatter count | Determines the number of acceptable input transitions that can occur
in a given time period before considering the input to be chatter. | C.Ptxx.ChatterCount | 2...127 Default value is 2. |
Chatter time | Determines the amount of time, from 1 through 10000 milliseconds,
within which the number of input transitions are counted. | C.Ptxx.ChatterTime | 1...10000 ms Default value is 1000 ms. |
Parameter | Description |
|---|---|
Diagnostics | Opens the diagnostics dialog box to view diagnostics information. |
Provide Feedback