PtXX - Counter view parameters

Input Filters
Parameter
Description
Member Name
Value
Off → On filter time
Specifies a value by which to delay the transition from Off to On. This delay is useful for filtering out transients in noisy environments.
C.Counterxx.InputOffOnFilter
  • 0 µs (default)
  • 5 µs
  • 10 µs
  • 20 µs
  • 50 µs
  • 100 µs
  • 200 µs
  • 500 µs
  • 1 ms
  • 2 ms
  • 5 ms
  • 10 ms
  • 20 ms
  • 50 ms
On → Off filter time
Specifies a value by which to delay the transition from On to Off. This delay is useful for filtering out transients in noisy environments.
C.Counterxx.InputOnOffFilter
  • 0 µs (default)
  • 5 µs
  • 10 µs
  • 20 µs
  • 50 µs
  • 100 µs
  • 200 µs
  • 500 µs
  • 1 ms
  • 2 ms
  • 5 ms
  • 10 ms
  • 20 ms
  • 50 ms
Counter
Parameter
Description
Member Name
Value
Preset
Displays the value set in the Output tag O.Counterxx.Preset member to use for counter preset.
0...2,147,483,647
Rollover at Preset
Causes the counter to rollover to zero at the Preset value.
  • If RolloverAtPreset is set, the counter counts to the Preset value, rolls over to zero, and then sets the Rollover bit. The Done bit is not set.
  • If RolloverAtPreset is not set, the counter sets the Done bit and continues counting up to Max DINT. The Rollover is set when Count transitions from 2,147,483,647 to 0.
C.Counterxx.RolloverAtPreset
0 = Cleared (default)
1 = Selected
Other
Parameter
Description
Diagnostics
Opens the diagnostics dialog box to view diagnostics information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal