PtXX Diagnostics - Output dialog box parameters

Parameter
Description
Value
Fault exists
Displays
Yes
if the device has a fault.
Yes or No
Data uncertain
Displays
Yes
if the device is operating outside the designed operating range, or if data is under manual or override control.
Yes or No
Short circuit fault
Displays
Yes
if the channel has a short-circuit or over-current fault.
Yes or No
Short circuit fault timestamp
Displays the timestamp of the last fault in
YYYY
-
MM
-
DD
-
HH
:
mm
:
SS
.
mmm
format.
  • YYYY
    = year
  • MM
    = month
  • DD
    = day
  • HH
    = hour (24 hour)
  • mm
    = minutes
  • SS
    = seconds
  • mmm
    = milliseconds
A valid time or no value if no event time was recorded.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal