Points view parameters
TIP:
The available parameters depend on the
Selected Mode
values specified in the Device Definition
dialog box.Parameter | Description |
|---|---|
Disabled Points | Displays the disabled points. This parameter is available only when at least one point is set to the Disabled mode. |
Enable FIFO event latching | Latches the on-board 256 events buffer by selecting this checkbox. |
Port | Indicates the port number for the channel. |
Point | Indicates the number of points to which the configuration applies. |
Mode | Indicates the mode assigned to the point. |
Output State During Program Mode | Specifies the behavior of each output when the controller's mode changes to Program. |
Output State During Communication Fault Mode | Specifies the behavior of each output when the connection from the controller to the output device is broken. |
Input Filter Time Off → On | Specifies the Off to On filter time to delay transitions from Off to On. Possible values include:
|
Input Filter Time On → Off | Specifies the On to Off filter time in milliseconds to delay transitions from On to Off.
|
Counter Preset | Displays the value set in the Output tag O.Counterxx.Preset member to use for counter preset. |
Counter Rollover at Preset | Determines the action taken when the data member I:Count reaches the O:Preset value.
|
Diagnostics | Opens the diagnostics dialog box to view diagnostics information. |
Provide Feedback