Overview view parameters
TIP:
The available parameters depend on the device being configured.
Parameters that do not apply to the device are hidden.
Parameter | Description |
|---|---|
Series | Indicates the series of the device. |
Revision | Indicates the major and minor revisions of the device. |
Electronic keying | Indicates the electronic keying for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs. Valid values are:
For more detailed information on Electronic Keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Points | Indicates the number of points to be configured. |
Connection | Indicates the connection format for the device. |
MAOC Compatible Data | Indicates whether the data is compatible with Motion Arm Output Cam (MAOC) instruction. If the data is not compatible with MAOC, you cannot use this device with MAOC instruction. This parameter applies to devices with major revision 2. |
Timestamp | Indicates the timestamp point assignment. |
Point Assignments | Displays the selected mode configured for each device point. |
Device definition | Opens the dialog box to change the revision, electronic keying, and other device specific values. |
Provide Feedback