Device Definition dialog box - Point Assignments parameters
Parameter | Description |
|---|---|
Port | Indicates the device port numbers. |
Point | Indicates the point to which this configuration applies. |
Selected Mode | Specifies the mode assigned to the point while offline. See Available Selected Mode values for the complete list of available
values. |
Fast | Indicates whether the point is a fast I/O point of the device. |
Provide Feedback