Change device type or revision
Use the
Change type
dialog box to change the
device type or revision.- On the tab for the device, select Overview.
- In the Overview view, select Device definition.
- In Device definition, select Change type.
- In Change type, in theTosection, specify the device type and revision as needed.TIP:Changing device type will change, delete, and/or invalidate the device properties that are not valid for the new device type.
- Select OK to finalize the changes and exit the dialog box.
Provide Feedback