Configuration view parameters

The
Configuration
view includes these parameters:
TIP:
For 1756 digital diagnostic input devices, if the connection is configured for Rack, the diagnostic configuration and I/O data are not supported; if the connection is configured for Data, the diagnostic configuration and I/O data are supported. The supported diagnostics are determined by the catalog number.
Parameter
Description
Input Filter Time
Specifies the value (in milliseconds) by which to delay the transition from off to on (
Off -> On
) and from on to off (
On -> Off
). This delay is useful for filtering out transients in noisy environments.
Enable Change of State for Diagnostic Transitions
Configures the device to transmit diagnostic status data with an updated timestamp as soon as the diagnostic data changes state. If this feature is not selected, the device transmits the diagnostic status data cyclically at the Requested Packet Interval (RPI) and does not update the timestamp.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal