Transmit diagnostic status data with a timestamp on state change
Configure the device to transmit diagnostic status data with an updated timestamp as soon as the diagnostic data changes state. If this feature is not selected, the device transmits the diagnostic status data cyclically at the Requested Packet Interval (RPI) and does not update the timestamp.
Prerequisites
- Make sure that the connection is configured for Data.
To transmit diagnostic status data with a timestamp on state change
- On the tab for the device, selectConfiguration.
- In theConfigurationview, selectEnable Change of State for Diagnostic Transitions.
- SelectOKto save the changes.
Provide Feedback