A non-zero chatter time requires a non-zero event value and vice-versa
For Chatter Detection, if you enter a non-zero value in the
No. of Events
column for any point, you must also enter a non-zero value in the corresponding Time
column. If you enter a non-zero value in the Time
column for any point, you must also enter a non-zero value in the corresponding No. of Events
column.Provide Feedback