Input Channels view parameters
The
Input Channels
view includes these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Input Type | Sets the input type for the channel. Available options are:
|
Input Range | Sets the input range for the input type. Ranges vary according to the selected Input Type . Available options are:
|
High Signal | Sets one of the four constants in the scaling equation. High Signal is in terms of the input signal units and corresponds to High Engineering when scaled.High Signal must be greater than Low Signal . |
Low Signal | Sets one of the four constants in the scaling equation. Low Signal is in terms of the input signal units and corresponds to Low Engineering when scaled. |
Units (Signal) | Shows the unit of measurement for High Signal and Low Signal . |
High Engineering | Sets one of the four constants in the scaling equation. High Engineering corresponds to High Signal and helps determine the engineering units that the signal values scale into. |
Low Engineering | Sets one of the four constants in the scaling equation. Low Engineering corresponds to Low Signal and helps determine the engineering units that the signal values scale into. |
Units (Engineering) | Shows the unit of measurement for High Engineering and Low Engineering and for the channel’s input value. |
Digital Filter | Specifies the time constant, in milliseconds, for a digital first order lag filter on the input. The digital filter smooths input data noise transients for the selected channel on the device. A value of 0 disables the filter. |
Disable Alarms | Determines whether process alarms are generated.
|
Real Time Sample (RTS) | Specifies how often, in milliseconds, the device scans its input channels. After the channels are scanned, the device multicasts the data. The selected Real Time Sample (RTS) period applies to the entire device. You cannot set a different value for each channel. The RTS period controls how often the device prepares new readings. The Requested Packet Interval (RPI) controls how often the device sends its current readings to the controller. Ideally the RTS and RPI should be identical so that each reading is sent to the controller only once at the time of sampling. |
Synchronize sampling with other devices | Allows all the 1756-IF4FXOF2F devices in a rack to synchronize the time in which samples are taken. The default is unchecked meaning no synchronization. |
Provide Feedback