Value is under range

One of these error conditions occurs:
Condition
Solution
ChX digital filter value under range. Value = 'xx', Minimum value = 0.
Enter a value greater than 0.
ChX user fault value under range. Value = 'x', Minimum value = -32768.
Enter a value greater than -32768.
RTS value under range. Value = 'xx', Minimum value = 'yy'.
Enter a value greater than the minimum value.
ChX program user defined value under range. Value = 'x', Minimum value = -32768.
Enter a value greater than -32768.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal