Value is over range

One of these error conditions occurs:
Condition
Solution
RTS value over range. Value = 'xx', Maximum value = 'yy'.
Enter a value less than the maximum value allowed.
ChX digital filter value over range.
Enter a value less than 20,099 ms.
ChX user fault value over range. Value = 'xx', Maximum value = 32767.
Enter a value less than 32767.
ChX rate limit value over range. Value = 'xx', Maximum value = 32767.
Enter a value less than 32767.
ChX program user defined value over range. Value = 'xx', Maximum value = 32767.
Enter a value less than 32767.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal