Invalid value
One of these error conditions occurs:
- Module filter (-3dB) value invalid.Verify the controller tag value is correct:Filter ValueController Tag Value10 Hz050 Hz160 Hz2100 Hz3250 Hz41000 Hz5
- ChX input range value invalid.Verify that the controller tag value is correct:RangeController Tag Value-10 V to 10 V00 V to 5 V10 V to 10 V20 mA to 20 mA3
- ChX output range value invalid.Verify that the controller tag value is correct:RangeController Tag Value-10 V to 10 V00 mA to 20 mA1
Provide Feedback