ChX ramp value too large

One of these conditions occurs:
Condition
Solution
ChX rate alarm value is too large.
Enter a value less than or equal to ((High Engineering – Low Engineering) * 2.1).
ChX ramp rate value is too large.
Enter a value less than or equal to ((High Engineering – Low Engineering) * 2.1).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal