ChX alarm value invalid

One of these error conditions occurs:
Condition
Solution
The high high limit value for the specified channel is less than the high limit value.
Enter a high high limit value that is greater than, or equal to, the high limit
value.
The low limit value
for the specified channel is less than the low low limit value.
Enter a low limit value that is greater than, or equal to, the low low limit value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal